Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for the line side terminal shields for the Powerpact Q-Frame breakers?

Issue:
Does Square D offer a lug shield for Powerpact Q-Frame breaker?

Product Line:
Circuit Breaker

Resolution:
The 2-pole shield is part number PKSB1Q2, and the 3-pole is part number QSB3.

NOTE: for the PowerPact Q-Frame breakers used in the 400amp Combination Service Entrance Devices, the Line Side Shields(or Barriers) will come with the CSED device from the factory.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings