Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the UL Standard and file number for the Homeline and QO load center generator interlock kits?
Issue:
Codes and Standards

Product Line:
Homeline Load Centers

Resolution:
The Homeline and QO generator interlock kits are considered load center accessories and do NOT obtain their own UL listing, BUT are tested and listed under the Load Center UL standard and file number. The load center standard is UL 67, "Standard for Safety - Panelboards". Additional UL standards may be referenced within UL 67 for compliance to that standard. The UL File is #E6294, Volume 7, Section 16.

NOTE: These generator kits will come with a wiring diagram that needs to be applied to the load center. They will also come with installation instructions and all the appropriate hardware.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings