Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement part number for the replacement mechanical interlock for the 8736SF** reversing starter?
Issue:
Replacement mechanical interlocks for NEMA Size 4 Starters

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Accessories

Resolution:
Depends on the specific device Class and Type. Select the appropriate interlock from description below:

For (2) 3 pole units horizontally arranged = 9999SM12
For (2) 3 pole units vertically arranged = 9999SM13
For (2) 4 pole units horizontally arranged = 9999SM12
For (2) 4 pole units vertically arranged = 9999SM13

See attached as reference

Schneider Electric USA

Attachment(s)
Mechanical interlocks.pdf [372.08 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings