Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Energy Efficient Transformers, such as the EX75T3H, available with K Factor ratings?
Issue:
Energy Efficient Transformers K ratings and suffix
Product Line:
LV Transformers
Environment:
Catalog Selection
Resolution:
Yes, the 2016 Department of Energy (DOE) Act includes Transformers for harmonic applications. The NP , NLP K rated Transformers for K9 HMT and K13 respectively) are available from SquareD/Schneider Electric.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings