Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are 9070 Type T or TF Industrial Control Transformers three phase or single phase?

Issue:
Use of Industrial Control Tranformers in Three Phase environments

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Industrial Control Transformers are used for relatively small power needs, no need for Three Phase versions

Resolution:

All 9070 Class T or TF type Industrial Control Transformers are Single Phase.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings