Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does Square D offer a 200A Switch at 12470V, 3 phase, outdoor use?
Issue:
200A Switch at 12470V offer for 3 phase outdoor use.

Product Line:
Switchgear

Environment:
North America Products

Cause:
N/A

Resolution:
Yes, Square D has the HVL/cc and HVL load interrupter switches. Information can be found on these in Section 9 of the Digest. There are outdoor HVL switches that can be ordered out of the Digest. HVL/cc Digest listed switches are only indoor.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings