Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the temperature rating of the main lugs used in ALL the MP Meter-Pak devices?
Issue:
Current product design features

Product Line:
MP meter pak metering

Resolution:
Main lugs used in ALL the MP Meter-Pak metering equipment are rated 75 degree C maximum. For use with Al or Cu wire having 90 degree C insulation in this equipment, the wire MUST be sized per the 75 degree C maximum listing in NEC Table 310-13.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings