Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Why isn`t AL100FD field installable on EDB, EGB, and EJB 15-30 A breakers anymore?
Issue:
Why isn`t  AL100FD field installable on EDB, EGB, and EJB 15-30 amp breakers anymore?

Product Lines:
E Frame, NF Panelboards

Resolution:
AL100FD is no longer a field installed option on the latest 15-30 A breakers due to a molding process change and associated rejection features.
AL100FD can be factory installed using suffix LH, like EDB34020LH.
CU100FD is still a field installable option for 15-30 A breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings