Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a PowerPacT P frame breaker's motor operator internal or external?
Issue:
Is the motor operator for a P-frame considered internal to the breaker or external?

Product line:
Molded case circuit breakers

Resolution:
It is internal and part of the mechanism of the breaker. It is replaceable, but not field installable on a breaker that did not come with a motor operator.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings