Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a 9065SFB20 be used on a 8536SCO size 1 starter?
Issue:
Can 9065SFB20 be used on Starters NEMA size 00,0 and 1?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S NEMA Starters

Resolution:
Yes. The 9065SFB20 will work on sizes 00, 0, and 1

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings