Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the Meter Barrier for use on 200/225 ampere, lever bypass METER-PAK and EZ METER-PAK branch devices, when the utility standards require barriers between meter positions.

Issue:
Product Design Features

Product Line:
Meter-Pak and EZM Metering

Environment:
Accessory

Cause:
Utility Requirement

Resolution:
When the Utility company requires a barrier between the meter sockets on the Commercial Lever Bypass Meter-Pak and EZM Metering Branch devices, use kit part number MML200BAR, kit includes (3) barriers. The kit can be used on the MPL and EZML 200 and 225amp Meter socket catalog numbers. See the attached instruction sheet for all the catalog numbers.

NOTE: THIS KIT DOES NOT GET USED AS BARRIERS BETWEEN TENANT BREAKERS IT IS ONLY FOR THE METER SOCKETS.

Schneider Electric USA

Attachment(s)
MML200BAR Instructions.pdf [99.75 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings