Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are there instructions on wall mounting a General Purpose Transformer? What grade of steel or bolts does should the customer use?
Issue:
Mounting Transformers

Product Line:
LV Transformer

Environment:
EX, EE Transformer

Resolution:
Square D/Schneider Electric can provide wall and ceiling mounting brackets for this purpose, but does not specify grade of bolts, type of wall fasteners or other mounting hardware.  A Local Structural Engineer should be called upon to determine what grade of bolts to use, and other Wall Structural Integrity questions etc.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings