Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal wire range for QBL, QDL, QGL, and QJL breakers?
Issue:
What wire size is accepted on QBL, QDL, QGL, QJL breakers?

Product Line:
Powerpact molded case circuit breakers

Resolution:
The terminal wire range is (1) #4 -300 kcmil Al or Cu. Replacement lugs are not available. The 250 A lugs are suitable for copper conductors only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings