Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the phasing of EZM, EZMR, EZMH, EZML, and EZMT branch units be changed in the field?
Issue:
What is the default phasing for 3 phase in, 1 phase out EZM branch unit?

Product Line:
EZM

Resolution:
Three Phase IN (208Y/120 VAC 3-Phase, 4-Wire) and Single Phase OUT (120/208 VAC 1-Phase, 3-Wire) Type: EZM, EZMR, EZMH, EZML and EZMT branch units are phased balanced at the factory as closely as possible and are capable of being altered on site to more accurately balance total connected loads on each phase.

3-Gang branch units are factory phased balanced with (1) A-B, (1) B-C & (1) A-C meter socket per position.  No additional balancing should be required.
4-Gang branch units are factory phased with (1) A-B, (1) B-C & (2) A-C meter sockets per device.  A meter center having multiple 4-Gang units is a candidate for additional phase balancing in the field.  This is easily accomplished by moving the meter socket LINE Side only  "Z-Shaped" connectors as needed to have an equal number of A-B, B-C & A-C meter socket positions.  Follow instructions provided on the wiring diagram to relocate these connectors in the field.

NOTE:  Applications requiring system voltage 240/120 VAC 3-Phase, 4-Wire High Leg Delta feeding of 120/240 VAC 1-Phase, 3-Wire tenants require use of branch units with Suffix  "CA" added to their catalog number (Example: EZM314225CA).  These High Leg Delta branch units will have all meter socket positions factory bussed to phases A-C and are not adjustable in the field.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings