Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is an SDM38VBIR?
Issue:
Product features

Product Line:
Multi-link structured wiring

Resolution:
The SDM38VBIR is a Square D Multi-Link Structured Wiring component. It is an amplified, bi-directional Video Hub, for use with CATV systems, used to distribute up to 3 video source signals to 8 TV outlets. One video source would be from the CATV system and two video sources would be modulated input sources from peripherals such as a VCR, DVD or satellite antenna. A 120Vac power supply is included.

NOTE: The Multi-Link Structured wiring product line is Obsolete, no longer available with NO replacement from SE.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings