Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H225DS, Series E2?
Issue:
Repair parts list for H225DS, series E2

Product Line:
Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN225AE2 (includes line and load base assembly, arc suppressor assembly, box insulator, line phase insulators, and mounting hardware)
Line base assembly - 4055221050SEL (2 required and arc suppressor assembly is not included)
Load base assembly - 4055221150SEL (2 required)
Arc suppressor assembly - 4051204501 (2 required)
Small lug Replacement- 4025113650 (aluminum; original lug was copper)
Large lug assembly - 4025602650 (1 required one per base assembly)
Line base phase insulator - 4051201401 (1 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051219150SEL
Vault handle - 4051219450SEL
Handle knob kit - 4028343550

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings