Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can two or three Single Phase Low Voltage dry type Distribution Transformers be Banked into a Three Phase Delta to Wye connection ?
Issue:
Can Single Phase Transformers be used together for 3 phase?

Product Line:
LV Transformers

Environment:
Applies to Distribution Transformers by SquareD/Schneider Electric

Resolution:
Yes.  This is one of the many options listed in the Dry Type Transformer Application Guide, document # 7400HO9501, reference page 9.  See the attached Handout.

Schneider Electric USA

Attachment(s)
Transformer application 7400HO9501.pdf [1.12 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings