Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does suffix 1416 indicate on a legacy circuit breaker?
Issue:
Define suffix 1416
Product Line:
Circuit Breakers
Resolution:
1416 is a combination suffix indicating a 24 Vdc shunt trip (1027), 2A/2B auxiliary contacts (1352), and a 1A alarm switch (2100).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings