Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for the closing caps used to cover the Main Horizontal cross bus openings in the Current design EZM Metering Devices?

Article available in these languages: Spanish

Issue:
EZM closing cap replacement part numbers.

Product Line:
Metering Equipment

Environment:
EZM Metering Equipment

Cause:
Maintenance

Resolution:
NOTE: The EZM Main Bus Closing Caps ONLY come with the Main Devices, they DO NOT come with the EZM Branch devices.


EZMCAP is the closing cap to cover the LEFT Side opening of an EZM device, it measures 2 inches in depth.
EZMSCAP is the closing cap to cover the RIGHT Side ONLY opening of an EZM device, it measures 1 inch in depth.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings