Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you install a SDSA1175, SDSA3650, QO21175SB or HOM2175SB TVSS unit in a Mini Power Zone MPZ type Transformer?

Issue:
Transient Voltage Surge Suppression products in Mini Power Zone Transformers (MPZ)

Product Line:
LV Transformers


Environment:
Applies to Mini Power Zone (MPZ) Transformer products from SquareD/Schneider Electric

Cause:
The application of a Mini Power Zone (MPZ) Transformer and specification of TVSS Transient Voltage Surge Suppression

Resolution:
No. The Mini Powerzone is not UL listed for the installation of any surge/TVSS unit inside the enclosure or in the loadcenter section.   However, TVSS Transient Voltage Surge Suppression may be connected external to the MPZ enclosure

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings