Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are heavy duty safety switches rated for grounded B phase applications?
Issue:
Corner-grounded delta application for Heavy Duty Safety Switches

Product Line:
Safety Switches​

Resolution:
Yes. Both fusible and non-fusible heavy duty safety switches 30 - 600 A are rated for use with grounded B phase applications. However, the 800 - 1200 A switches are NOT suitable for use with a grounded B phase/corner grounded delta voltage system.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings