Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
On a U-line starter, how does the auto reset work?
Issue:
How does the auto reset function works on a Tesys U motor starter?

Product Line:
IEC Contactors and Starters

Environment:
Tesys U Starters

Resolution:
In Auto Reset mode, the U-line starter (with an Advanced Control Unit and the LUFDA10 function module) operating handle remains in the "ready" position but the coil is de-energized and the power poles open on an overload. After a motor cool-down, the unit resets and the power poles close. Proper wiring is essential

On a short circuit fault, the handle moves and the device will have to be manually reset.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings