Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for an optional main lug kit that will accept 2-500 kcmil per phase for a 400 amp main lug NF Panel?
Issue:
Main lugs option

Product Line:
Panelboards

Environment:
NF

Cause:
Larger 500kcmil cables

Resolution:
The NALV4 compression lug kit is an optional main lug kit which will accept 2-500 kcmil wires per phase for a 400 amp main lug NF Panel but only for the pre-series E1 panel

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings