Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for a filler plate for a JDL,QBL type subfeed breaker being removed from an NQOD or NQ panel?

Issue:
Catalog number for a filler plate for a JDL,QBL type subfeed breaker being removed from an NQOD or NQ panel.

Product Line:
Lighting and appliance panelboards

Environment:
NQOD and NQ

Cause:
Maintenance

Resolution:
The filler plate for NQOD panel Sub feed breaker opening has been obsoleted and a 3rd Party will need to fabricate a cover for this opening.
For NQ panel sub feed breaker openings, a Blank NQ?RDE rail extension kit where ? = dimensions high the blank trim and rail extension are.
For example NQ6RDE is for a 6" blank trim that is 20"W x 6"H . NQ12RDE = a 12" H x 20"W rail extension. See attached Bulletin

Schneider Electric USA

Attachment(s)
NQ Rail ext inst bulletin 80043-732-02.pdf [7.07 MB]
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings