Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does a Surge Supression device such as a TVS2EBA24A require a circuit breaker or other means of disconnect? If so, what amperage?
Issue:
Does a Surge Supression device such as a TVS2EBA24A require a circuit breaker or other means of disconnect?  If so, what amperage?

Product Line:
Surge Protection.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
To protect a TVS2EBA24A, you may use a 3 pole, 30A (minimum) breaker, although a 60A breaker is preferred.


CTA-ID : 2035521

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings