Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a QE7 breaker a good type?
Issue:
Has a breaker with a QE7 stamp on it and wanted to know if that's the part number ?

Product line:
MCCBS MEDIUM OFFER

Resolution:
That is a UL designation only. The breaker is a standard QE type. QE breakers are obsolete without replacement.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings