Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CH364AWK, series F5? (may be shown as F05)
Issue:
Repair parts list for CH364AWK, series F5

Product Line:
Safety Switches

Resolution:
The replacement parts for the CH364AWK, series F5 (F05) are as follows. No other parts are available.
-Complete Line Base - 4056703550 (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
-Line Base mounting screws - 4020546401 (6 required per line base)
-Load Base Assembly - 4056678250 (1 required per phase; includes phenolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020546401 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - CL20F (includes 6 lugs; requires mounting screws below)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
-Switch Mechanism mounting screws - 2299940562 (2 required)
-Handle Assembly - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings