Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are QMB branch switches provided with the mounting hardware necessary to install it into the QMB panelboard?
Issue:
Is there any special tools , or hardware needed to install a QMB switch into a QMB Panelboard / Switchboard QMB distribution?

Product Line:
Panelboards / Switchboard QMB distribution

Environment:
QMB Switches.

Cause:
Installation/Feature

Resolution:
The Current E Series units are shipped with all the necessary screws and hardware to mount the side flanges to the sides of the enclosure.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings