Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the VISI-TITE bolt used in old style (Series 1, 2, or 3) EZ Meter-Pak be replaced in the field?
Issue:
Repair Parts

Product Line:
Obsolete EZM

Resolution:
No. Old style EZM made use of a sliding joint-pak and a single VISI-TITE two headed joint bolt in each cabinet. Once the outer head of this VISI-TITE Bolt was broken off (at the first installation), a second hex head remains that can now be used as a normal bolt. A label near the bolt head indicates the proper torque to be applied the next time this sliding joint-pak needs to be reinstalled.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings