Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the torque spec for the AL100FD lugs?
Issue:
Torque requirement for terminal lug on EDB, EGB, and EJB breakers

Product Line:
NF Panelboard Breakers

Resolution:
For #14 - #10 AWG Al/Cu, it is 35 lb-in. For #8 - 2/0 AWG Al/Cu, it is 50 lb-in.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings