Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the Line Side terminal lug data for ALL the Combination Service Entrance Devices and the Specified torque requirements for the lugs?
Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Terminal Line side lug data

Resolution:
CSED = Combination Service Entrance Device

ALL the Line Side Terminal lug data for each CSED can be seen in the current digest pages(see below for an example visual). Also, this information is on the CAD drawing for each device and is located on the wiring diagram that is attached to each device from the factory.
Link to CAD dwg search by catalog number

The specified torque requirements for the Line Side Lugs can be found on each device Wiring Diagram attached to each device from the factory.



Digest table


Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings