Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do I select a Buck Boost Transformer for a direct-connected motor load?

Issue:
Selection of Buck Boost Transformers for Motor Loads

Product Line:
LV Transformers


Environment:
Applies to Buck and Boost Transformers by SquareD/Schneider Electric


Cause:
Motor Loads can have high inrush or Locked Rotor Current when starting


Resolution:
Buck Boost units can be sized based on the full load current and voltage differential. Since the impedance presented to the circuit by the Autotransformer connection is low, a locked rotor current condition will not cause a large IZ voltage drop across the Transformer(s).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings