Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the purpose of SO2040BAR, used with combination service entrance devices?
Issue:
Product design Features

Product Line:
Combination Service Entrance Devices

Resolution:
The SO2040BAR is a wireway barrier kit that can be used in conjunction with the SO2040M200S combination service entrance device. This would also be pertinent to SO2040VP, a value pack that includes the SO2040M200S. A new interpretation of the utility designated space and customer designated space has impacted the use of the SO2040M200S. This interpretation only affects panels sold within Arizona, Nevada, and California. This wireway barrier must be field installed on this product if it is to be energized in the above states whose utilities are part of EUSERC.

The purpose of this kit is to prevent load wiring from being routed through the channels beside the enclosed meter socket. If the SO2040M200S is to be installed in areas outside of EUSERC, where they are utility approved, these wireway barriers may not be required.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings