Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for a replacement main lug kit for an HCM50916 I-Line interior?
Issue:
Catalog replacement for  main lug kit for an HCM50916 I-Line interior.

Product Line:
Panelboard

Environment:
HCM50916

Cause:
N/A

Resolution:
That I-Line interior will require a catalog number 80116-122-50 quantity of (3) for the main lugs, and one (1) for the neutral assembly, if necessary.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings