Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a RC200S, Series M03?
Issue:
Current design repair parts

Product Line:
Combination Service Entrance Device

Environment:
Repair parts

Cause:
maintenance

Resolution:

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 7329410450
Main Breaker Section Cover - 7329410550
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 7329420101 (also requires insulator and rivets, below)
Dead Front Interior Trim Insulator - 4053435601 (attaches to rear of interior trim)
Dead Front Interior Trim Insulator Rivets - (2) 2430313230
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one screw is required)
Meter Base Assembly - 4056250050 (includes meter base, (2) line side lugs, (4) meter jaws, (4) meter jaw blade guides, and load side bussing)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Fifth Jaw Kit - 5J
Closing Cap - (2) ACP
Main Breaker - QOM2-VH type, 200 A maximum
Main Breaker Mounting Nuts - (2) 2342702001
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings