Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the EZM metering equipment be used on 240 Vac 3-Phase, 3-Wire electrical systems?
Issue:
Can the EZM Devices be used with a 240Vac Delta system?

Product Line:
EZM Metering Equipment

Resolution:
NO, the EZM metering equipment is designed only for the following electrical systems:
120/240 Vac, 1-Phase, 3-Wire
208Y/120 Vac, 3-Phase, 4-Wire
240/120 Vac DELTA, 3-Phase, 4-Wire
EZM metering equipment is not available for use on 240 Vac DELTA, 3-Phase, 3-Wire electrical systems.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings