Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are EDB, EGB, and EJB circuit breakers rated at 50 Hz?
Issue:
Are the E-frame breakers for NF panelboards rated at 50 Hz?

Product Line:
Circuit Breakers

Resolution:
Yes, they are 50/60 Hz rated.

Note: Only the standard breakers are 50/60 Hz rated. The EPD breakers are 60 Hz only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings