Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a 400 A commercial EZM branch meter socket that meets the EUSERC specifications available?
Issue:
Product availability

Product Line:
EZM Metering

Resolution:
No, there are no 400 A EZM branch devices with test block bypass that meet the EUSERC specifications. A 225 A branch is the maximum. For 400 A, consider switchboards or CT cabinets.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings