Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where can an EZM600FTLK3 feed-thru lug kit be used and what wire ranges will it accommodate?
Issue:
Application

Product Line:
EZM

Resolution:
The EZM600FTLK3 feed-thru lug kit is suitable for use only in 800 A EZM-TB tap boxes (EZM1800TB, EZM3800TB, EZM1800TBCU, and EZM3800TBCU).
Kit includes (4) lugs per phase and neutral and all mounting hardware.
Lug wire range is (1) 1/0 AWG - 750 kcmil Al/Cu, or (2) 1/0 AWG - 300 kcmil Al/Cu.

Schneider Electric USA

Attachment(s)
EZM600FTLK3 Instruction Bulletin.pdf [512.02 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings