Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can any of the CSED all-in-one or meter main devices be converted from a ring to a ringless type meter socket or vice versa?
Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Resolution:
No, the designs of the ring and ringless meter socket covers will not allow a ring type device to be changed to a ringless type device, nor visa versa. There would also be an issue with the National Electrical Code, Article 110.3(B), Listing and Labeling.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings