Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum amperage available for the horizontal ganged meter product line and are they available with disconnects for each meter?
Issue:
Product Design Features

Product Line:
Horizontal Gang Metering

Resolution:
The horizontal ganged meters are available with a maximum of 200 A meter sockets. BUT they are NOT available with disconnects for each meter socket. Metering devices that contain disconnects are available in the MP Meter-Pak line and EZM metering.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings