Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Has the red LED been removed on the 9065 Motor Logic Solid State overloads?
Issue:
Why the red LED was removed on the 9065 Motor Logic Solid State overloads?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)

Resolution:
Yes. The Power On LED served no useful purpose and therefore has been removed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings