Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the meter socket(s) in the MPL Meter-Pak devices be temporarily bypassed around the watt-hour meter?
Issue:
Can we bypass the MPL Meter-Pak devices temporarily?

Product Line:
Metering Equipment

Resolution:
Yes, MPL style Meter-Pak meter centers are supplied with lever type bypass and jaw release on each meter socket. The bypass feature is ONLY for use on a temporary basis and ONLY by the local utility company and is NOT suitable for continuous duty service. Once the lever bypass is engaged, the lever handle extends beyond the front surface of the enclosure, preventing the ringless style meter socket cover from being installed. After the lever handle is disengaged, the meter socket cover can be installed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings