Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there an adaptor plate available that would allow the use of a Series A style hub in place of a Series A-L style hub?
Issue:
Is it possible to use a Series A style hub on a Series A-L hub opening?

Product Line:
Circuit Breaker Enclosure

Resolution:
Yes. The AAP adaptor plate allows a Series A style hub to be used on a device that is setup for a Series A-L style hub.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings