Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
If Square D type NF panels are rated for 480Y/277V, what are the 600V EJB breakers such as catalog number EJB36030 for?
Issue:
What is the purpose for the 600V EJB breakers such as catalog number EJB36030?

Product Line:
Panelboards

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The the E frame 600V breakers are for Canadian applications for Canadian NF panels using a 600/347V system.


CTA-ID : 2037588

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings