Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for a Series 1, QMB306T branch switch?
Issue:
Product Replacement

Product Line:
QMB Branch Switches

Environment;
Replace Obsolete Device

Cause:
Application or Maintenance

Resolution:
It will depend on the QMB panelboard age and type. But the QMB322TD Series D2 switch can be used, provided that the QMB interior was manufactured after 1961 and before October 1984. The series D2 switch will come standard with rail extensions, BUT a QMB306LEX plug-on extension kit is required if the QMB panel is a Type QW (38-inch wide) manufactured before 1984 and and has flat bus bars. For visuals of the QMB interiors see the current Supplemental Digest pages for Obsolete Panelboards.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings