Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the Homeline circuit breakers be used at 50 Hz?
Issue:
Homeline breakers for use in 50Hz

Product Line:
Miniature Circuit Breakers

Resolution:
Yes, the standard thermal/magnetic HOM breakers are rated for both 50 and 60 Hz systems. However, the electronic breakers (DF, AFI, CAFI, GFI, etc.) are rated for 60 Hz only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings