Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the EX/EXN mounting accessories have seismic rating?
Issue:
Seismic Rating of WMB and CMB accessories

Product Line:
LV Transformers

Environment:
Applies to Transformer Wall Mounting Brackets from SquareD/Schneider Electric

Cause:
Transformers must often be wall mounted

Resolution:
None of the wall mounting brackets for the Square D/Schneider Electric transformer product line are seismically rated on their own. The seismic rating of the transformer remains when these accessories are properly installed/bolted to the transformer but the installation/mounting seismic approval would have to be given by the structural engineer or local inspector who will check the conformity of the installation according to local requirements.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings