Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where can the 3 tier series short circuit current rating (SCCR) information be located for EZM metering devices and load centers?

Article available in these languages: Spanish

Issue:
Is there a document that shows the SCCR for EZM metering devices and load centers?

Product Line:
EZM Metering

Resolution:
The 3 tier series short circuit current rating (SCCR) can be found in the Product Data Bulletin 4100DB0301 (see below attached). This bulletin can be located on-line in the Square D Technical Library, under load centers. It is also, possible to Google the Bulletin number and view it. In addition, the load centers will have as standard attached to the covers a 3-Tier SCCR label that will show the 3 tier ratings.

Schneider Electric USA

Attachment(s)
LC SCCR Bulletin Final Released 3-2014.pdf [2.29 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings