Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the CSED catalog number RC2040M200CGP contain?
Issue:
Product features

Product Line;
Combination Service Entrance Devices

Resolution:
This catalog number contains the standard CSED catalog number RC2040M200C with a factory installed RCGK2 Generator Interlock Kit. A HOM230 is used as the back-fed generator main breaker. This device is labeled "Suitable for use as transfer equipment in accordance with Article 702 of the National Electric Code ANSI/NFPA 70".

Note: This catalog number is mainly available through Retail Outlets

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings